Where to change drive strength for USB 3.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to change drive strength for USB 3.0?

1,628 Views
parth_modi
Contributor I

Hi All,

We are working on imx8mq processor-based custom design. We used Linux kernel 4.14 for development. We want to change the drive strength of USB 3.0 USB2 port.

The pins are following to needs to change drive strength.

USB2_DN
USB2_DP
USB2_TX_P
USB2_TX_N
USB2_RX_P
USB2_RX_N

Can you please share documents or file name to change this drive strength of USB2 port?

Thanks,
parth

0 Kudos
Reply
1 Reply

1,490 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Parth,

Please check register PHY_CTL3_ADDR, fields TXRESTUNE0 and TXRISETUNE0.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply