Where to change ddr training file in uboot 4.14.78_ga

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to change ddr training file in uboot 4.14.78_ga

3,474 Views
killro89140
Contributor II

Hi All,

NOTE : this is quite a long question, I apologize and thank for answering first. Thanks!

We used u-boot, kernel with 4.9.88 and 4.9.123 on imx8mq-evk board before,

and recently, we update both our u-boot and kernel to 4.14.88.

It works with default parameter, and original micron lpddr4 3GB DRAM.

However we face to some issue with different setup below.

1. ddr folder disappeared in u-boot ver. 4.14.88.

      In 4.9.88 and 123, we generate our ddr_init.c and ddr4_training.c files and put it to 

      /board/freescale/imx8mq_evk/ddr/ folder, in order to customize our speed an timing.

      However, we found that ddr folder is removed from ver 4.14.88, we did found that there is a new 

      folder called /board/freescale/imx8mq_arm2/. and inside it having ddr/ddr4/ folder, 

      which include ddr_init.c and ddr_traing.c files. But not sure it's the correct place to replace the files.

      

      Another thing relate to this one is that, we found from ver4.9.123 and above( including 4.14.88), 

      driver/ddr/imx8m/ was created, however, 4.9.88 didn't having this driver ! 

      Moreover, in the driver having lpddr4_training.c (not ddr4_training.c)and ddr_init.c.

      Again, maybe here is the place to replace ?

2. Bug? DDR Stress Tool V21 can only generate ddr4_init.c and ddr4_training.c for ver 4.9.51?

      When we using Stress tool to Gen the training file.

      If we using "CODE" mode,  it will gen the code with comment said it's 2017 for 4.9.51.

      When we compared it with origin ddr4_* code in u-boot ver 4.14.78 source code, there are pretty different !

      So, we doubt that v21 can support ver 4.14.78 or not?

      If we using "ARRAY" mode. it will come out with lpddr4_timing.c file, 

      which used in ver4.14.78, in folder ./board/freescale/imx8mq_evk/ , and read by driver/ddr/imx8m/ddr4_init.c.

      It seems it did the same thing of ./board/freescale/imx8mq_evk/ddr/ddr_init.c when it was ver 4.9.88/123,

      but with for loop.

      Maybe this is the correct way to set DRAM setting registers for lpddr4 + ver 4.14.78 u-boot ??

      (and ddr_init.c / ddr_training.c is no longer used in 4.14.78? )

3. Does ddr4 and lpddr4 setting and operation been separated in v4.14.78?

      Like I mentioned above, it seems NXP is trying to separate the lpddr4 setting from ddr4.

      Could anyone advise what's the lpddr4 setting and related code in ver4.14.78 ? 

      It seems ddr4 and lpddr4 were not separated clearly now, and quite confused...

      since in old version they using the same training file and init file as well as driver.

BTW, It seems imx8 stuff was created step by step in newer version, which is great.

We confused that we can't find imx8m code in old version, which only having imx7 and imx6 code.

Anyway, thanks for reading, hope someone can answer the question.

Best regards,

Edwin

0 Kudos
Reply
2 Replies

2,795 Views
igorpadykov
NXP Employee
NXP Employee

Hi Edwin

seems changes should be in uboot/board/freescale/imx8mq_evk/lpddr4_timing_b0.c
lpddr4_timing_b0.c\imx8mq_evk\freescale\board - uboot-imx - i.MX U-Boot 

and it is explained in MSCALE_DDR_Tool_User_Guide.pdf included in

ddr test package, in particular p.3-13, Figure 3-8 Generated Code Format  ‘ARRAY’ format

i.MX8 MSCALE SERIES DDR Tool Release (V2.10) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,795 Views
killro89140
Contributor II

Hi Igor,

Thanks for reply, 

Ok, I see , it said,

Choose ‘CODE’ format or ‘ARRAY’ format from the dropdown list. Please choose ‘ARRAY’ format for the latest u-boot SPL driver. If you are using old u-boot code or study the complete DDR initialization flow, please choose ‘CODE’ format.

Which means ddr4_init.c and ddr4_training.c is not used for uboot v4.14.78,

while lpddr4_timing.c, which gen from DDR Tool, is going to replaced the lpddr4_timing_b0.c ?

But, in document, it just copy the lpddr4_timing.c  instead of lpddr4_timing_b0.c 

Step1b. If you are using xxx_timing.c in new version of u-boot

$ cd uboot-imx
$ cp directory_to generated_code/lpddr4_timing.c board/freescale/imx8mq_evk/

Best regards,

Edwin

0 Kudos
Reply