Where is the i.MX8QM chip configuration?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the i.MX8QM chip configuration?

Jump to solution
923 Views
YukioOyama
Contributor III

Hello,

The i.MX8QM reference manual sometimes says to see  the chip configuration. However, there is no chip configuration in either the reference manual or the datasheet. Where is the chip configuration shown?
I am now interested in the relationship between the temperature sensor and the ADC in the chip.

YukioOyama_0-1687241540031.png

 

Best Regards,

Yukio Oyama

 

0 Kudos
Reply
1 Solution
894 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
4 Replies
907 Views
joanxie
NXP TechSupport
NXP TechSupport

pls check the enclosed file

0 Kudos
Reply
903 Views
YukioOyama
Contributor III

Hello Joanxie-san,

Thanks for quick reply.

According to your documentation, the ADC only reads two temperature sensors.

Linux thermal management monitors five: the A53 and A72 cores, the two GPU temperatures, and the PMIC temperature. The PMIC temperature is probably read from the PMIC via some interface. The remaining four are the temperatures within the i.MX8.

The temperatures within the i.MX8 would be read out to which register? Not this ADC register?


I am not going to read the temperatures directly from the registers in my application. I ask this question to know how the hardware works.

Best Regards,

Yukio Oyama

0 Kudos
Reply
895 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
887 Views
YukioOyama
Contributor III

Hello joanxie-san,

I see that the temperature was monitored by SCU. Thanks for letting me know.
That's all I have to ask. I will close the case.

Best Regards,

Yukio Oyama

 

0 Kudos
Reply