Where is the i.MX6 Platform SDK?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where is the i.MX6 Platform SDK?

1,712 次查看
cbrust
Contributor III

The following link appears broken and I cannot find the i.MX6 Platform SDK to which it points.  https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&Parent_nodeId=133...​​

Has the SDK's name/location changed and is it still available or ... something else?

Thanks in advance.

cliff

标签 (4)
0 项奖励
回复
1 回复

1,300 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The Platform SDK for i.MX6 was removed since it is not supported more.

Please create SR to get it if needed.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复