Where is the i.MX6 Platform SDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the i.MX6 Platform SDK?

1,043 Views
cbrust
Contributor III

The following link appears broken and I cannot find the i.MX6 Platform SDK to which it points.  https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&Parent_nodeId=133...​​

Has the SDK's name/location changed and is it still available or ... something else?

Thanks in advance.

cliff

Labels (4)
0 Kudos
1 Reply

631 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The Platform SDK for i.MX6 was removed since it is not supported more.

Please create SR to get it if needed.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos