Where is the document that is named Freescale U-Boot User’s Guide?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the document that is named Freescale U-Boot User’s Guide?

Jump to solution
1,063 Views
ko-hey
Senior Contributor II

Hi all Please tell me the place of the document. In P7 of Freescale Yocto Project User's Guide (Rev L3.10.17_1.0.0-ga), there is a description as below. However, I can not find it from community and Freescale Web site. "For more information on Uboot configuration, see the Freescale U-Boot User’s Guide." Please tell me !! Best Regards,

Labels (3)
0 Kudos
Reply
1 Solution
712 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

please refer to attached document Chapter 1.

All released documents are included in Doc bundle:

L3.10.17_1.0.0_LINUX_DOCS Linux 3.10.17 BSP & MM Bundle

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
713 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

please refer to attached document Chapter 1.

All released documents are included in Doc bundle:

L3.10.17_1.0.0_LINUX_DOCS Linux 3.10.17 BSP & MM Bundle

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
712 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for quick reply.

Do you mean that there is a no document that is named "Freescale U-Boot User's Guide” ?

Were the document integrated to "Freescale Yocto Project User's Guide” ?

Best Regards,

ko-hey

0 Kudos
Reply
712 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

you are right, there is no such document.

Best regards

igor