Where is the document that is named Freescale U-Boot User’s Guide?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where is the document that is named Freescale U-Boot User’s Guide?

跳至解决方案
1,311 次查看
ko-hey
Senior Contributor II

Hi all Please tell me the place of the document. In P7 of Freescale Yocto Project User's Guide (Rev L3.10.17_1.0.0-ga), there is a description as below. However, I can not find it from community and Freescale Web site. "For more information on Uboot configuration, see the Freescale U-Boot User’s Guide." Please tell me !! Best Regards,

标签 (3)
0 项奖励
回复
1 解答
960 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

please refer to attached document Chapter 1.

All released documents are included in Doc bundle:

L3.10.17_1.0.0_LINUX_DOCS Linux 3.10.17 BSP & MM Bundle

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
961 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

please refer to attached document Chapter 1.

All released documents are included in Doc bundle:

L3.10.17_1.0.0_LINUX_DOCS Linux 3.10.17 BSP & MM Bundle

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
960 次查看
ko-hey
Senior Contributor II

Hi Igor

Thank you for quick reply.

Do you mean that there is a no document that is named "Freescale U-Boot User's Guide” ?

Were the document integrated to "Freescale Yocto Project User's Guide” ?

Best Regards,

ko-hey

0 项奖励
回复
960 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

you are right, there is no such document.

Best regards

igor