Where is the default config file?

cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the default config file?

560 Views
Contributor I

I used imx7d CPU and got a code of linux-imx_4.1.15-r0. I used bitbake to compile the code. I want to know which default config of the project be used? I change the file at folder of sources/meta-fsl-arm/recipes-kernel/linux/linux-imx-4.1.15/imx/defconfig. But it doesn't effect.

0 Kudos
1 Reply

22 Views
NXP TechSupport
NXP TechSupport

Hello,

  generally it is recommended to follow i.MX_Yocto_Project_User's_Guide.pdf

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Also You may look at

Yocto Training - Task #5 

Changing the Kernel configuration for i.MX6 SABRE 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos