Where is the DDR3 calibration code that is excerpted in AN4466?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the DDR3 calibration code that is excerpted in AN4466?

993 Views
bikenomad
Contributor IV

I'd like to get the DDR calibration values for our new board.

App note AN4466 shows an excerpt from some code, but it's not complete.

Is there a ready-to-go code example that I could add to my hacked version of OBDS that runs from internal RAM only to get these values?

Labels (1)
0 Kudos
Reply
2 Replies

687 Views
petertaylor
Contributor II

Ned,

Did you ever get an answer for this?  What did you do?  I'm at the same point and wanting to test the DDR3 calibration. 

Peter

0 Kudos
Reply

687 Views
TomE
Specialist II

New Document dated this month (April 2014):

http://cache.freescale.com/files/training/doc/ftf/2014/FTF-SDS-F0170.pdf

"DRAM Controller Optimization for i.MX"

There's a lot of good information in this document on setting up RAM to run on i.MX5 and (mainly) i.MX6.

Tom

0 Kudos
Reply