Dear All,
We are using LCD which requires initialization over SPI. I was referring to drivers/video/mxc/mxcfb_epson_vga.c driver available from Kernel 3.0.35. But we are using latest 3.10.17 kernel and it seems this driver is not available in latest kernel.
Can anyone let me know where can I get similar reference ported on kernel 3.10.17?
Regards,
Dipen Patel
Hi Dipen
seems it is not used on any i.MX6 boards,
I think one can look at wandboard with SEIKO-WVGA or boundary devices
examples
How to use future electronics LCD display and adapter with Wandboard?
http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/
Best regards
igor
Dear Dipen,
Do you have any idea whether drivers/video/mxc/mxcfb_epson_vga.c is a ADC or SDC framebuffer driver. Because in the driver they have commented like "MXC Frame buffer driver for SDC" , but the Asynchronous IPU functions are getting used in the driver.
For eg: ipu_init_async_panel(ipu, 0, IPU_PANEL_SERIAL, 90, IPU_PIX_FMT_GENERIC, sig);
Thanks in Advance ..:smileyhappy: