Where is USB OTG documentation for i.MX6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is USB OTG documentation for i.MX6?

ソリューションへジャンプ
1,886件の閲覧回数
shefft
Contributor IV

2

I'm looking for a software guide on setting up OTG in host mode.  The reference manual lacks enough information and the Freescale Platform SDK is broken so I need to know where the guide is that explains how to use the OTG port (i.e. how to configure the registers correctly).  Can you Freescale guys points me in the right direction?

0 件の賞賛
返信
1 解決策
1,498件の閲覧回数
shefft
Contributor IV

1

Host mode problem is solved.  My Nitrogen6X board has a PMIC for OTG power that needs to be activated using a GPIO pin.  Also, a device must be plugged in for the port to register as enabled in the PORTSC1, which seems weird.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,499件の閲覧回数
shefft
Contributor IV

1

Host mode problem is solved.  My Nitrogen6X board has a PMIC for OTG power that needs to be activated using a GPIO pin.  Also, a device must be plugged in for the port to register as enabled in the PORTSC1, which seems weird.

0 件の賞賛
返信
1,498件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

I see, good to know that for the Nitrogen board !.

0 件の賞賛
返信
1,498件の閲覧回数
shefft
Contributor IV

1

What would cause Port Enable to be low when Port Power is high?

0 件の賞賛
返信
1,498件の閲覧回数
shefft
Contributor IV

1

The specific problem I'm seeing is the OTG PORTSC1 register PSPD (speed) bits read Undefined.  There is no reason for this, as the init sequence looks fine and the registers look correct.  The sequence works fine for the other host controller ports, and when the Freescale boot ROM sets the OTG up for serial image download, this problem does not occur.

0 件の賞賛
返信