Hi,
On the dowload page, there are L3.0.101_4.1.1_SOURCE_BSP and L3.0.101_4.1.1_SOURCE_BSP but not L3.10.17_1.0.2_SOURCE_BSP
I am not using Yocto but buildroot, and I need
firmware-imx-xx.gz, xserver-xorg-video-imx-viv-xx.tar.gz ... where can I find them please ?
Regards
Thierry
Thanks !
The sources are loaded from repositories. Please use Release notes in
http://cache.freescale.com/files/32bit/doc/support_info/IMX6YOCTOPATCHRN.pdf
Demo images :
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------