Hi George
you are right, mclk is affected as described on
https://community.nxp.com/message/922214?commentID=922214#comment-922214
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi George
please read carefully suggested link, it summarizes:
"in conclusion audio_mclk_root_clk clock is taken all the time by SAI1.."
So it is used for mclk generation.
Best regards
igor
Hi Igor,
This issue is still not 100% clear to me, also not from the referenced old post.
If AUDIO_MCLK_CLK_ROOT is used by SAI1, then is SAI1_CLK_ROOT never used ? Or are both clock roots needed ?
If both are needed, from which root clock is the bit clock derived ?
Best regards,
Hans