Where is ADDR_TRANSLATION_SUPPORT_EN set, for the PCIe ATU?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is ADDR_TRANSLATION_SUPPORT_EN set, for the PCIe ATU?

566 Views
shefft
Contributor IV

Using iMX6Solo - Figure49-24 shows different options for the ATU.  One key selector in the diagram is the ADDR_TRANSLATION_SUPPORT_EN bit.  It is not mentioned by this name anywhere else in the document.  So what is it?  Where to find it?

Labels (1)
0 Kudos
1 Reply

427 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The ADDR_TRANSLATION_SUPPORT_EN bit relates to PCIe IP, which is
embedded in i.MX6 SOC, and strictly speaking it should be removed from

i.MX6 Reference Manual.

http://read.pudn.com/downloads153/ebook/670795/DWC_pcie_reference.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos