Where i download freescale toolchain and linux rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where i download freescale toolchain and linux rootfs

Jump to solution
3,436 Views
aravinthkumarja
Senior Contributor II

Hi all,

I need freescale toolchain download link.?

i need freescale Linux BSP rootfs alone download link.?

Regards,

Aravinth

0 Kudos
1 Solution
1,941 Views
igorpadykov
NXP Employee
NXP Employee

Hi aravinthkumar

please follow steps described on p.5 attached Freescale_Yocto_Project_User's_Guide.pdf or

check gcc collection for example on:

http://repository.timesys.com/buildsources/g/gcc/

Current gcc version is decribed on p.9 Release Notes.

Ready for use roots can be found in Demo images:

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
1,942 Views
igorpadykov
NXP Employee
NXP Employee

Hi aravinthkumar

please follow steps described on p.5 attached Freescale_Yocto_Project_User's_Guide.pdf or

check gcc collection for example on:

http://repository.timesys.com/buildsources/g/gcc/

Current gcc version is decribed on p.9 Release Notes.

Ready for use roots can be found in Demo images:

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,941 Views
czur
Contributor III

Hi Igor,

Can you please recommend the toolchain we can go for for imx6sx, Is it better to compile the toolchain using yocto/buildroot? or is it better to download the Linaro/GCC prebuilt?

Thanks

Arun

0 Kudos