Where could I buy a display screen that supported by i.MX6Q board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where could I buy a display screen that supported by i.MX6Q board?

Jump to solution
1,788 Views
hzc
Contributor I

Thank you!

0 Kudos
1 Solution
1,596 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX6Q support the follows display. Which one do you want? LVDS Screen or others? And here could tell me which board are you using? Our reference board or the board you design yourself?

Display

  • 10.1" 1024 x 768 LVDS display with integrated P-cap sensing
  • HDMI connector
  • LVDS connector (for optional second display)
  • LCD expansion connector (parallel, 24-bit)
  • EPDC expansion connector (i.MX 6DualLite only)
  • MIPI DSI connector (two data lanes, 1 GHz each)


Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
12 Replies
1,596 Views
kentlowman
Contributor I

FDI is a long term "Partner of NXP" and we offer our ELI, Easy LCD Interface, Family of products to provide customers a plug and play embedded touch screen display option for i.MX6 and other Single Board Computers.

ELI Highlights

* Only 3 connections needed: HDMI, USB for touch and Power

* Quick time to market, distribution stock

* 10 year channel life

* 4.3" to 15.0" display sizes

See this link for a video of ELI plug and play capability with NXP  iMX7D SABRE Kit:

   https://www.youtube.com/results?search_query=teamfdi+eli

See this link for more info on the ELI Family:

   http://www.teamfdi.com/eli

Thanks,

Kent Lowman

0 Kudos
1,597 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX6Q support the follows display. Which one do you want? LVDS Screen or others? And here could tell me which board are you using? Our reference board or the board you design yourself?

Display

  • 10.1" 1024 x 768 LVDS display with integrated P-cap sensing
  • HDMI connector
  • LVDS connector (for optional second display)
  • LCD expansion connector (parallel, 24-bit)
  • EPDC expansion connector (i.MX 6DualLite only)
  • MIPI DSI connector (two data lanes, 1 GHz each)


Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,596 Views
hzc
Contributor I

Thank you very much!

My board is this one:

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/arm-mcus-and-mpus/i....

I have built Andorid 6.0 according to the 

And the Android 6.0 is running successfully。

My problem is I have no available display. 

I clicked the link found that it was a device, not a single display screen.

Where is the LVDS or LCD link?

Which one I can use without porting display or touching driver?

0 Kudos
1,595 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You are using the i.MX6Q-SDP board, here you can directly using the LVDS screen. The link is :i.MX53 Quick Start Board|NXP  you can see the LVDS screen MCIMX-LVDS1. Or you can also using the HDMI screen without porting.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,595 Views
hzc
Contributor I

Many thanks!

0 Kudos
1,596 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome. It's my pleasure. If you have new questions you can create new threads in our community.

Here could you help close this thread by click the Mark Answer button. Thanks.

Have a nice day

Rita

0 Kudos
1,596 Views
hzc
Contributor I

Sorry, I forgot a question.

Dose this screen support touching? and do I need modify any driver?

0 Kudos
1,596 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the i.MX6Q-SDP board board?

0 Kudos
1,596 Views
hzc
Contributor I

Yes.

0 Kudos
1,596 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The android BSP on the i.MX6Q-SDP board support LVDS screen disply and touching. You do not need to modify any diver. You can see all the features about the android BSP suppoting in the document Android_Release_Notes. Here I attach it for you.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,596 Views
hzc
Contributor I

Thanks a lot!

0 Kudos
1,596 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

It's my pleasure~~

0 Kudos