Where can we find the clock requirement specification of i.MX6 Solo Lite?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can we find the clock requirement specification of i.MX6 Solo Lite?

ソリューションへジャンプ
622件の閲覧回数
m_c
Senior Contributor I

Such as tolerance (+-PPM), CL... of 24M & 32.768k.

ラベル(1)
タグ(2)
0 件の賞賛
1 解決策
513件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to section 1.7 (Oscillator tolerance)

of “Hardware Development Guide for i.MX 6SoloLite - User Guide” :

"The following table provides 24 MHz oscillator tolerance guidelines

(see Table 1-7, recommendations #4 and #5). Because these are guidelines,

the designer must verify all tolerances per the official specifications".

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
514件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to section 1.7 (Oscillator tolerance)

of “Hardware Development Guide for i.MX 6SoloLite - User Guide” :

"The following table provides 24 MHz oscillator tolerance guidelines

(see Table 1-7, recommendations #4 and #5). Because these are guidelines,

the designer must verify all tolerances per the official specifications".

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛