Where can we find the clock requirement specification of i.MX6 Solo Lite?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can we find the clock requirement specification of i.MX6 Solo Lite?

Jump to solution
1,092 Views
m_c
Senior Contributor I

Such as tolerance (+-PPM), CL... of 24M & 32.768k.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
983 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to section 1.7 (Oscillator tolerance)

of “Hardware Development Guide for i.MX 6SoloLite - User Guide” :

"The following table provides 24 MHz oscillator tolerance guidelines

(see Table 1-7, recommendations #4 and #5). Because these are guidelines,

the designer must verify all tolerances per the official specifications".

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
984 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to section 1.7 (Oscillator tolerance)

of “Hardware Development Guide for i.MX 6SoloLite - User Guide” :

"The following table provides 24 MHz oscillator tolerance guidelines

(see Table 1-7, recommendations #4 and #5). Because these are guidelines,

the designer must verify all tolerances per the official specifications".

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply