Where can we find DDR stress test for i.MX25?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can we find DDR stress test for i.MX25?

1,103 Views
m_c
Senior Contributor I

Customer found some issues when booting i.MX25 from SPI NOR flash under -40℃ like 1) no message output after decompress Linux kernel, 2) kernel panic with different error message in each boot. There is no such issues in previous version which boot from parallel NOR flash. Customer is checking the hardware difference and want to check DDR stability in the mean time.

Labels (1)
0 Kudos
Reply
1 Reply

944 Views
Yuri
NXP Employee
NXP Employee

Hello,

   We do not have special DDR stress test for i.MX25 (as for i.MX6 and i.MX53). Sorry.

You may try to decrease DRAM frequency to check if memory is the main problem for system

stability. Also different drive strength options for both i.MX25 and DRAM parts may help.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------