Where can we find DDR stress test for i.MX25?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where can we find DDR stress test for i.MX25?

656 次查看
m_c
Senior Contributor I

Customer found some issues when booting i.MX25 from SPI NOR flash under -40℃ like 1) no message output after decompress Linux kernel, 2) kernel panic with different error message in each boot. There is no such issues in previous version which boot from parallel NOR flash. Customer is checking the hardware difference and want to check DDR stability in the mean time.

标签 (1)
0 项奖励
回复
1 回复

497 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   We do not have special DDR stress test for i.MX25 (as for i.MX6 and i.MX53). Sorry.

You may try to decrease DRAM frequency to check if memory is the main problem for system

stability. Also different drive strength options for both i.MX25 and DRAM parts may help.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------