Where can one find the i.MX5x Ubuntu 10.04 image (i.MX53 SABRE)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can one find the i.MX5x Ubuntu 10.04 image (i.MX53 SABRE)

954 Views
kriszawada
Contributor III

I am following a document called "i.MX5x Ubuntu 10.04 Startup Guide" (i.MX5x_EVK_Ubuntu_10.04_StartupGuide.pdf) and in section 4.1 is mentions a file named "imx53_smd_L2.6.35_11.05.01_ER_demo_image.gz", but I cannot find this file on the i.mX53 SABRE website.  I want t

Has anyone ran into this before?  Is it expected that the user creates this image?

Screenshot.png

Labels (2)
0 Kudos
Reply
2 Replies

718 Views
SergioSolis
NXP Employee
NXP Employee

Hello Kris,

you can find the file in the following link:

SABRE Platform for Tablets based on i.MX53 Product Summary Page

Under:

Operating System Software - Board Support Packages  >> L2.6.35_MX53_ER_1105_IMAGE

0 Kudos
Reply

718 Views
kriszawada
Contributor III

Hello SerchMX,

Ok, I see what you mean by downloading L2.6.35_MX53_ER_1105_IMAGE.  However, once I click on this link it takes me to a download of:

L2.6.35_11.05.01_ER_images_MX5X.tar.gz

After extracting the above file I get a file named:
L2.6.35_11.05.01_ER_images_MX5X.tar

I have extracted the file above and now I see :

\---L2.6.35_11.05.01_ER_images_MX5X

    |   amd-gpu-x11-bin-mx51_11.05.01-1_armel.deb

    |   atheros-wifi_11.05.01-1_armel.deb

    |   firmware-imx_11.05.01-1_armel.deb

    |   imx-lib_11.05.01-1_armel.deb

    |   imx-test_11.05.01-1_armel.deb

    |   kernel_2.6.35.3-imx_11.05.01_armel.deb

    |   libz160-bin_11.05.01-1_armel.deb

    |   modeps_11.05.01-1_armel.deb

    |   rootfs.ext2.gz

    |   rootfs.jffs2

    |   u-boot-mx50-ddr2.bin

    |   u-boot-mx50-lpddr2.bin

    |   u-boot-mx50-mddr.bin

    |   u-boot-mx50-rd3.bin

    |   u-boot-mx50-rdp.bin

    |   u-boot-mx51.bin

    |   u-boot-mx53-ard-ddr3.bin

    |   u-boot-mx53-ard.bin

    |   u-boot-mx53-loco.bin

    |   u-boot-mx53-smd.bin

    |   u-boot-mx53.bin

    |   udev-fsl-rules_11.05.01-5_armel.deb

    |   uImage

    |   xserver-xorg-video-imx_11.05.01-1_armel.deb

    |   zImage

    |

    \---chromium_os

            firmware-imx-2011.05.01.tar.bz2

            imx-lib-2011.05.01.tar.bz2

            kernel-2011.05.01.tar.bz2

            libz160-2011.05.01.tar.bz2

            modeps-2011.05.01.tar.bz2

            opengles-2011.05.01.tar.bz2

            u-boot-2011.05.01.tar.bz2

            udev-fsl-rules-2011.05.01.tar.bz2

            xserver-xorg-video-imx-2011.05.01.tar.bz2

However, I do not specifically see the file "imx53_smd_L2.6.35_11.05.01_ER_demo_images.gz".

Sincerely,

Kris

0 Kudos
Reply