As title, does anyone know where the source code for the executables in the LTIB "unit_tests" directory can be found?
I was trying to build ltib from scratch in the hope that that would provide me with the source code but it appears to be massively deprecated and practically impossible to build.
Thanks,
Ralph
解決済! 解決策の投稿を見る。
please try
"L3.0.35_4.1.0_ER_SOURCE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Source Code Files"
and refer to attached sources
Best regards
igor
Hi ralph_
please refer to p.10 attached document
./ltib -m prep -p <package name>
for imx-test package ("unit_tests")
./ltib -m prep -p imx-test
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Okay, so I got a load of missing packages from http://www.bitshrine.org/gpp/, copied them to my /opt/freescale/pkgs directory and ran the command like you said and it demands that I enter a "Platform choice". There is no option for the i.MX6. What do I do?
Here are the options it gives me:
Future Designs, Inc. ARM9DIMM-LPC3250 board
senTec COBRA5475 Coldfire/M68k (MMU)
Embedded Artists 3131 board with the NXP LPC313X SoC
Embedded Artists 3152 board with the NXP LPC3152 SoC
Embedded Artists LPC3250 OEM Board with the NXP LPC32XX SoC
EP93xx development board
Freescale IMX21 ADS reference board
Freescale IMX27 ADS reference board
Freescale IMX31 ADS reference board
Logic PD LPD7A404 board
Freescale M5208EVB Coldfire/M68k (noMMU)
Freescale M5253EVB Coldfire/M68k (noMMU)
Freescale M532xEVB Coldfire/M68k (noMMU)
Freescale M537xEVB Coldfire (noMMU)
Freescale M5445X Coldfire/M68k (MMU)
Freescale MCF547x_8x Coldfire/M68k (MMU)
Freescale MPC512x based boards
Freescale MPC5200 based development boards
Freescale MPC7448HPCII PPC development board
Freescale MPC82xx based development boards
Freescale MPC8349EA MDS PowerPC board
Freescale MPC8349E-mITX board
Freescale MPC8360E PB PowerPC board
Freescale MPC837xE MDS development board
Freescale MPC8536DS PowerPC development board
Freescale MPC8548CDS PPC development board
Freescale MPC8555CDS and MPC8541CDS PPC development board
Freescale MPC8560ADS PQ3 PowerPC board
Freescale MPC860FADS
Freescale MPC8641DHPCN PPC development board
Phytec 3250 board with the NXP LPC32XX SoC
A&MLtd Adder MPC875 PowerPC board
Raspberry Pi with BCM2835 SoC
TQ Components TQM823L PowerPC board
Please use
"L3.0.35_4.1.0_ER_SOURCE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite and i.MX 6Solo Linux BSP Source Code Files"
and install all packages suggested in attached file.
After a fairly epic struggle I finally got LTIB built. For anyone reading, whatever you do don't download rpm-4.0.4.tar.gz from the RPM website. Download it from the http://www.bitshrine.org/gpp/ website.
Should I be downloading the file L3.0.101_4.1.1_141016_source.tar.gz as well as this seems more recent than the file you suggested?
Thanks,
Ralph
yes L3.0.101_4.1.1_141016_source.tar.gz is latest -
download it and read carefully how to install it
using docs inside it.
Best regards
igor
Okay, but there don't seem to be any instructions inside. All I get is this:
ls L3.0.101_4.1.1_141016_source
firmware-imx-3.0.101-4.1.1 gpu-viv-bin-mx6s-3.0.101-4.1.1 imx-vpu-lib-3.0.101-4.1.1 ltib_config_platform_imx.patch patches
glib2-2.12.1-atomic.patch gpu-viv-wl-bin-mx6s-3.0.101-4.1.1 linux-3.0.101 ltib_dist_lfs-5.1.patch