Where are the NatureDSP unit tests?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where are the NatureDSP unit tests?

1,582 Views
abdob
Contributor III

Hi, 

This DSP User's guide:

https://www.nxp.com/docs/en/user-guide/IMX_DSP_USERS_GUIDE.pdf

refers to the unit_tests in this location:

Unit test location: rootfs: /unit_tests/DSP/naturedsp_test

Where can I find the unit tests? I've tried downloading and extracting the packages in the user guide, but I don't see the unit_tests directory anywhere.

Thanks,
Abdo

0 Kudos
Reply
5 Replies

1,572 Views
joanxie
NXP TechSupport
NXP TechSupport

firstly download images to your board, then you can find this when board boot up

"https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat..."

0 Kudos
Reply

1,566 Views
abdob
Contributor III

I was able to extract the rootfs from the I.MX 8M Plus EVK and I.MX 8QuadMax MEK images, I see /unit_tests/DSP directory however it only contains dsp_rend_test.out and dsp_test.out.

I don't have the actual boards but I am attempting to reuse the test vectors for the MIMRT685 EVK which includes the HIFI4 DSP but is not a linux-based board.

Is the content inside naturedsp_test accessible without having the linux-based boards?

0 Kudos
Reply

1,560 Views
joanxie
NXP TechSupport
NXP TechSupport

the user guide you refer to is for i.mx processor, if you are interested with IMXRT, pls create a new thread and put it in the i.mxRT community, the IMXRT engineer would check this for you, I'm not sure this package is available for imxRT or not

0 Kudos
Reply

1,548 Views
abdob
Contributor III

Hi, 

Although I have the i.mxrt board, I am running HIFI4 DSP examples using simulation.

This question is independent of the specific NXP board, I posted the question in this i.MX forum because the document refers to the DSP unit_test which I don't see present in the downloads mentioned.

I would appreciate it if I get any pointers to locate the unit tests.

Thanks,
Abdo

0 Kudos
Reply

1,542 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the user guide,

"NatureDSP Library package is license restricted on the i.MX platform. License authorization is required from the NXP marketing for the users to access the source code."

this package is under NDA, so pls contact local representative to get further help, we couldn't share any license restricted packages on the public community

0 Kudos
Reply