Where I find the DDR package trace lengths/delays for the i.MX7Dual?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where I find the DDR package trace lengths/delays for the i.MX7Dual?

622 Views
oscar_duran
Contributor I

Hi everybody,

I need to route a DDR3 memory for an i.MX7Dual (MCIMX7D7DVK10SD especifically) processor, but I can't to find the DDR package trace lengths/delays for this processor, an also I need to know if the package traces are symmetric or not.

Thank you for your answer in advance.

Labels (2)
Tags (2)
0 Kudos
1 Reply

559 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Oscar Duran,

When working on the layout using the i.MX7D please refer to the i.MX7 Hardware Design Guide (link below, you may need to login to download this file).

https://www.nxp.com/webapp/Download?colCode=IMX7DSHDG

Section 3.4 explains the routing rules for DRAM. These recommendations allow to have a robust design. The lengths given are measured from the processor pin to the DDR chip. The package trace lengths are not provided as they are similar enough on all pins to be disregarded when working on the frequencies supported by the processor.

I hope this helps!

Regards,

0 Kudos