Hi Community.
I saw RM and noticed. CM4F core in IMX8MM has CM4 ALIAS Code Region(262016KB).
I want to kown which DDR area does map the CM4 ALIAS Code.
Now, Our firmware is running on DDR(0x7F000000 - 0x80000000).
Can this be mapped to 0x10000000-?
--
By the way, breakpoints in the debugger are behaving strangely, as in the next thread.
https://community.nxp.com/message/1254243?commentID=1254243#comment-1254243
Best Regards,
T.Kashiwagi
解決済! 解決策の投稿を見る。
Hi Takashi
yes alias is fixed.
Corrected:
As answered on other post the alias maps to 0x40000000.
So "correct answer" on this post was changed.
Thanks Renato !
Best regards
igor
Hi Igor-san
Thank you.....
Hi Takashi
seems it is aliased to 8000_0000 - 8FFE_FFFF.
I am afraid it is not possible to remap to 0x10000000.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello @igorpadykov ,
According to your other post the alias maps to 0x40000000.
Please fix the "correct answer" on this post.
Thanks!
Renato
Hi Igor-san
Thank you for reply.
seems it is aliased to 8000_0000 - 8FFE_FFFF.
I am afraid it is not possible to remap to 0x10000000.
Is this aliased address(8000_0000 - 8FFE_FFFF) really fixed?
Our SoM has only 1GB Memory(0x40000000 - 0x7FFFFFFF)........
Best Regards,
T.Kashiwagi
Hi Takashi
yes alias is fixed.
Corrected:
As answered on other post the alias maps to 0x40000000.
So "correct answer" on this post was changed.
Thanks Renato !
Best regards
igor