Where CLK(input) come from ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where CLK(input) come from ?

ソリューションへジャンプ
974件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I'm using i.MX6Solo and  have questions about uSDHC controller.

According to Figure 67-2 of RM, Async FIFO use a clock that selected from CLK(input) or CLK(output).

Where CLK(input) come from ?

And how can user select CLK(input) or CLK(output) ?

ko-hey

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
886件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Terms CLK, DATA[7:0], and CMD relate to SD interface. In this sense

the CLK(input) is not used on i.MX6 uSDHC. CLK(output) is SD clock,

please refer to section 67.4.5 (Clock Generator) of the RM how it is generated. 

  Also, the base clock is the peripheral clock  ipg_clk (from ipg_clk_root), mentioned
in Table 67-5 (uSDHC Clocks) of the RM.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
887件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Terms CLK, DATA[7:0], and CMD relate to SD interface. In this sense

the CLK(input) is not used on i.MX6 uSDHC. CLK(output) is SD clock,

please refer to section 67.4.5 (Clock Generator) of the RM how it is generated. 

  Also, the base clock is the peripheral clock  ipg_clk (from ipg_clk_root), mentioned
in Table 67-5 (uSDHC Clocks) of the RM.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
886件の閲覧回数
ko-hey
Senior Contributor II

Yuri

Thanks.

ko-hey

0 件の賞賛
返信