When using LVDS LCD in 6-bit mode (Continued)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When using LVDS LCD in 6-bit mode (Continued)

ソリューションへジャンプ
1,900件の閲覧回数
george
Senior Contributor II

 

Hi All,

This post is a question related to the recent post. (https://community.nxp.com/t5/i-MX-Processors/When-using-LVDS-LCD-in-6-bit-mode/td-p/1326316)

The LCD specifications we want to use are, for example, the products at the following URL. https://www.avnet-integrated.eu/fileadmin/user_upload/Files/Displays/Colour_TFT/LQ150X1LG98.pdf

According to the specifications of these LCDs, it is recommended to fix the TX3 +/- differential data to 0 when using in 6-bit mode.

We have confirmed the i.MX6 specification, but it seems that the data output from the TX3 +/- cannot be kept fixed at 0 (or 1).

Please tell me what TX3 +/- will look like when using 6bit mode.
*We checked it with our product and the TX3 +/- buffer output pin may be floating

aaa.png

*LCD Datasheet P.11 shown in the URL

 

Best Regards,

George.

0 件の賞賛
返信
1 解決策
1,887件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

 

there are no special settings for keeping TX3 +/- differential data to 0, so if that solution

does not work, suggest to set necessary levels externally by resistors.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,888件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

 

there are no special settings for keeping TX3 +/- differential data to 0, so if that solution

does not work, suggest to set necessary levels externally by resistors.

 

Best regards
igor

0 件の賞賛
返信
1,870件の閲覧回数
george
Senior Contributor II

Igor,

Thanks.

0 件の賞賛
返信