When i use the 1000M ethernet phy AR8033 on imx6q sabresd platform on android 5.1,the 1000M ethernet cann't be reachable. The 1000M ethernet can be reachable on imx6 android 4.4.
The phenomenon is as follows:
Now I don't know why!
But i doubt it is the problem of tx clock delay or rx clock delay
I don't know if IMX6 platform has any settings about tx clock delay or rx clock delay
Can you give some advise for me?
Thanks
Hi tang
unfortunately in IMX6DQ/SDL platforms there are no rgmii settings for tx clock delay or rx clock delay.
One can try to recompile from scratch new image for android 5.1.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
You mean that it need to download the latest source code about android 5.1 and recompile the new image.