When i download the linux image to imx8mmini,the system cann't startup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When i download the linux image to imx8mmini,the system cann't startup

857 Views
tangyuan
Contributor III

Hi,

    When i download the linux image to imx8m mini,the system cann't startup

    The download command is as follows:

    1.png

The system information is as follows:

2.png

3.png

4.png

Please ,help me !Thank you 

Labels (1)
0 Kudos
2 Replies

766 Views
igorpadykov
NXP Employee
NXP Employee

Hi tang

what board used in the case, if this is custom board first necessary

to run ddr test

i.MX 8M Family DDR Tool Release 

and follow Chapter 4 How to bring up a new MX8MSCALE board MSCALE_DDR_Tool_User_Guide.pdf
included in ddr test package.

If this is EVK board follow Linux L4.14.98_2.0.0 Documentation

Linux Guide and use Linux Binary Demo Files - i.MX 8MMini EVK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

767 Views
tangyuan
Contributor III

My board is imx8 mini evk.I don't know the reason!

0 Kudos