Hi community,
Our customer have a simple question.
=====
[Question]
Would you let me know the condition when i.MX6DQ judges as POR_B is released?
When POR_B input voltage reaches to VIH (VDD_SNVS_IN * 0.7)?
Or when it exceeds VIL (VDD_SNVS_IN * 0.3)?
=====
Actually, POR_B slew rate on their custom board is very low (slope is gentle) to expand POR_B assertion time for ERR007926 workaround.
However, if i.MX6Q judges as POR_B is released when POR_B voltage exceeds VIL, their workaround is not enough.
In fact, they have to start mass production soon, so they want to clear it ASAP.
I would appreciate it if you could give us reply rapidly.
Best Regards,
Satoshi Shimoda
解決済! 解決策の投稿を見る。
Hi Satoshi
POR_B is released when POR_B input voltage exceeds VIH (VDD_SNVS_IN * 0.7).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
POR_B is released when POR_B input voltage exceeds VIH (VDD_SNVS_IN * 0.7).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------