Hi community,
Our patner have a question about i.MX6DQ VDD_SNVS_IN.
Please see footnote 2 of Table 8 in IMX6DQCEC.
According to this footnote, we understand i.MX6DQ VDD_SNVS_IN consume 1mA only when i.MX6DQ power-up and power supply voltage can supply 1mA.
On the other hand, Table 4-1 in IMX6DQ6SDLHDG Rev.1 says as following.
=====
According to table 13 of the chip data sheet, VDD_SNVS_IN can draw up to 1 mA depending on the application.
For those cases, an external regulator is needed because the PF0100 VSNVS regulator supplies 400 μA.
=====
According to this notes, i.MX6DQ consume 1mA not only when power-up but also when a application is runnning.
So we are confused by these description to understand when i.MX6DQ consume 1mA.
Would you let me know when i.MX6DQ VDD_SNVS_IN consumes 1mA what function in SNVS consume a lot of current to understand it?
This information will help us to judge whether MMPF0100A can be used for supply VDD_SNVS_IN or other LDO is required.
Best Regards,
Satoshi Shimoda
解決済! 解決策の投稿を見る。
Hi Satoshi
additional current when application is runnning may occur
in case described in Table 2-6 IMX6DQ6SDLHDG Rev.1
that is when VDD_SNVS_IN > VDD_HIGH_IN && VDD_HIGH_IN > 2.4V (typ.)
and current associated with loads connected to PMIC_ON_REQ, PMIC_STBY_REQ outputs.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
additional current when application is runnning may occur
in case described in Table 2-6 IMX6DQ6SDLHDG Rev.1
that is when VDD_SNVS_IN > VDD_HIGH_IN && VDD_HIGH_IN > 2.4V (typ.)
and current associated with loads connected to PMIC_ON_REQ, PMIC_STBY_REQ outputs.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your reply.
> that is when VDD_SNVS_IN > VDD_HIGH_IN && VDD_HIGH_IN > 4.5V (typ.)
Excuse me, what is 4.5V (typ.)? Is this typo of 2.4V (typ.)?
Best Regards,
Satoshi Shimoda
Hi Satoshi
you are right, correct is 2.4v(typ.)
Best regards
igor