When i.MX6 AUDMUX uses both Normal Mode and Internal Network Mode.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

When i.MX6 AUDMUX uses both Normal Mode and Internal Network Mode.

跳至解决方案
776 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6Q AUDMUX.

They want to confirm whether Port 1 and Port 2 output data during Port 7 output data in the following case.

Port 1 --(Normal Mode for I2S)--> Port 6

Port 2 --(Normal Mode for I2S)--> Port 5

Port 7 --+--(Internal Network Mode)--> Port 4

              |--(Internal Network Mode) --> Port 3

In this case, if Port 1 and Por 2 are in Internal Network Mode, these are not able to output data during Port 7 output data.

But these are in Normal Mode, it is no problem, right?

Best Regards,

Satoshi Shimoda

标签 (6)
标记 (1)
0 项奖励
回复
1 解答
605 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think you are right, Port 1 and Port 2 should be used in

Normal Mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
606 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think you are right, Port 1 and Port 2 should be used in

Normal Mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复