When changing dual lite to dual.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When changing dual lite to dual.

Jump to solution
1,042 Views
JHY
Contributor IV

I want to put i.mx6 dual on my dual lite board.

Maybe those two parts have pin-compatibility.

Please advise to me easy to miss for these jobs.

Labels (2)
0 Kudos
Reply
1 Solution
971 Views
b36401
NXP Employee
NXP Employee

Actually these processor are commonly pin-to-pin compatible.

For the details you can refer Hardware Design Application Note I attached.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
972 Views
b36401
NXP Employee
NXP Employee

Actually these processor are commonly pin-to-pin compatible.

For the details you can refer Hardware Design Application Note I attached.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply