When I run the same QT program and video (using mplayer)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When I run the same QT program and video (using mplayer)

1,693件の閲覧回数
jongjupark
Contributor I

Dear community,

 

When I run the same QT program and video (using mplayer)
The video did not appear on the QT program, but the video covered the entire QT program.
Normal operation should be as shown in [normal operation] screen.

Why is this happening?

 

**description**

Kernel Version : L3.14.28

Application : QT

[Normal operation] : Samsung Exynos4412 Cpu, Kernel 3.8

movie_exynos.jpg

[Abnormal Operation] : NXP IMX6Q, Kernel 3.14.28

movie_nxp.jpg

ラベル(6)
0 件の賞賛
返信
1 返信

1,601件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jongju

one can try to follow sect.8.4 Qt 5 attached Linux Guide,

also please check useful link

I.MX-6 - Qt Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信