When I Patch Code for i.MX, the result is not correct.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When I Patch Code for i.MX, the result is not correct.

1,050 Views
amychou
Contributor I

I do the all 3.1 Getting Android source code (Android/kernel/U-Boot).

And according to the document 3.2 Patch code for i.MX

Apply all the i.MX Android patches by performing the following steps:

1. Assume you have unzipped the i.MX Android release package to /opt/android_L5.0.0_1.0.0-ga_source .

$ cd ~/myandroid

$ source /opt/android_L5.0.0_1.0.0-ga_core_source/code/l5.0.0_1.0.0-ga/and_patch.sh

$ help

The result is as following.

Invoke ". and_patch.sh" from your shell to add following functions to your environment:

-- c_gotop:    Changes directory to the top of the tree

-- c_patch:    Recover working tree to base version and then applying FSL android patch

It looks incorrect.

Any steps missing?

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

790 Views
amychou
Contributor I

I also do the following step, and make sure I have permission to access the directory.

2.2 Unpacking the Android release package

After you have set up a computer running Linux OS, unpack the Android release package by using the following commands:

# cd /opt (or any other directory where you placed the android_L5.0.0_1.0.0-ga_core_source.tar.gz file, but make sure you have permission to access that directory;

otherwise, c_patch cannot work properly)

Thanks.

0 Kudos
Reply