What will be the address for uboot in serial NOR flash if using SPI programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What will be the address for uboot in serial NOR flash if using SPI programmer

887件の閲覧回数
adityanagal
Contributor III

HI ,

I am using IMX6 solo based target board  where IMX6 solo is interfaced with NOR Flash over SPI. I want to write uboot /kernel/roofs directly over NOR Flash using SPI programmer. At what addresses , uboot /kernel/rootfs need to be written over the serial NOR Flash.

Please suggest.

Regards,

Aditya Nagal

0 件の賞賛
返信
1 返信

715件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

please check ucl2.xml for SCM mfg tools (it has option for writing image to spi-nor)


Mfg Tool
Updates and Patches (2)
SCM-i.MX 6Dual/6Quad Manufacturing Toolkit for Linux 3.14.52 Patch Release (REV 1)
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?f...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信