What values of decoupling capacitors are used in PF0100 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What values of decoupling capacitors are used in PF0100 ?

1,957 Views
madhuwesly
Contributor I

Hello community,

I am designing a development board with iMX6Q as SoC and PF0100 as power management ic

I have referred the sabre board schematics(rev C5) and PF0100 datasheet. In sabre board schematics, they haven't used the decoupling capacitors values suggested by the PF0100 datasheet.

Can anyone tell me what decoupling capacitor values should I choose in my design?  

Attaching the sabre board schematics file.

PF0100 Datasheet link: http://www.nxp.com/assets/documents/data/en/data-sheets/MMPF0100.pdf  

Best regards

Madhu 

Labels (2)
0 Kudos
Reply
2 Replies

1,855 Views
art
NXP Employee
NXP Employee

Use the bulk capacitance scheme, shown on the i.MX6Q SABRE SD board schematic. It is proven to work.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,855 Views
madhuwesly
Contributor I

Hi artur,

Thanks for your reply. Will follow the bulk capacitance scheme provided by  i.MX6Q SABRE SD board schematic.

Best regards

madhu

0 Kudos
Reply