What the relation of sleep mode in hardware?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What the relation of sleep mode in hardware?

1,147件の閲覧回数
wangvictor
Contributor III

Hi All,

I'm trying to using the sleep mode and wake it on the enternet(wol).

For sleep mode I'm using this commend : echo mem > /sys/power/state

For my hardware I have to understand how is sleep mode doing with the hardware.

To know that my hardware is support to this ability or not.

Anyone can give me the suggestion?

Or any document to let me read.

Thanks in Advanced!

ラベル(7)
タグ(3)
0 件の賞賛
返信
1 返信

998件の閲覧回数
b36401
NXP Employee
NXP Employee

In sleep mode PLLs and crystal oscillator are disabled.
As for Linux details you can refer to i.MX 6 Linux Reference Manual:
https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信