What the NOR flash supports imx6 processor for downloading U-boot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What the NOR flash supports imx6 processor for downloading U-boot?

1,358 次查看
rustemkhakimov
Contributor I

Hi,

What the NOR flash supports imx6 processor for downloading U-boot?

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,067 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Gary has given the reply to you. Here you can refer to our i.mx6 reference board design in our community. You can refer to the board design in our website i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP . There are 32M nor falsh and 4M nor flash in our reference design.

M29W256GL7AN6E

M25P32-VMW3TGB

Have a nice day

Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,067 次查看
gary_bisson
Senior Contributor III

Hi,

You can have a look at the BD-SL-i.MX6 (SabreLite) schematics/documentation since it boots from NOR:

https://boundarydevices.com/product/sabre-lite-imx6-sbc/ 

The part used is the SST25VF016B.

Regards,

Gary