What should be the tCL value for this DDR3 memory ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What should be the tCL value for this DDR3 memory ?

3,698件の閲覧回数
peteramond
Contributor V

Hi All,

I'm referring to the attached ddr init script and could you please help me to fill it correctly ?

My memory is  AS4C256M16D3A-12BCN data sheet attached here with. 

Processor i.MX6Q

1) What should be the tCL value for this memory ? I can't find it in data sheet.

pastedImage_1.png

2) Can you please check this script and tell me whether it is correct or not for my memory module ?

Regards,

Peter. 

ラベル(4)
5 返答(返信)

3,422件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

 The parameter tCL of the i.MX6 Reference Manual really is CAS Latency, defined as the

delay, in clock cycles, between the internal Read command and the availability of the first

bit of output data. The overall Read Latency (RL) is defined as Additive Latency (AL) + CAS Latency (CL);

RL = AL + CL.

    The CAS latency is programmable value. It may be recommended to leave its value without changing,

as in the (Excel) tool suggested. Note, tCL may depend on DDR frequency and the same value must be

used in i.MX6 MMDC and DRAM part (in Mode Register MR0).

  From DRAM Datasheet, Table 2 (Speed Grade Information), recommended CL is 11 clocks for 800 MHz

memory device, meaning 13.75 ns; for 400 MHz, 13.75 ns is 6 clocks.

  In the (Excel) table, 7 is taken for assurance.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

3,422件の閲覧回数
peteramond
Contributor V

Yuri

Thank you very much for your feedback. 

Then what should be the tCWL value for the Excel table ?

pastedImage_1.png

Is that same as tCL ?

Could you please help me on this ?

Regards,

Peter.

0 件の賞賛
返信

3,422件の閲覧回数
Yuri
NXP Employee
NXP Employee

 Generally it is possible to have different CAS latencies for read and write operations. 

Good practice is to leave this parameter as the Excel table recommends.

~Yuri. 

3,422件の閲覧回数
peteramond
Contributor V

Yuri

Thank you. But it is saying obtain this value from ddr data sheet. I cant see tCWL value in data sheet. 

Is that okay to leave it as 6 ?

Regards,

Peter.

0 件の賞賛
返信

3,422件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The memory Datasheet states about 11 clocks for 800 MHz.

Therefore  the values of the tool are quire reasonable for specific (400 MHz)

configuration.

~Yuri.

0 件の賞賛
返信