Hi All,
I can see in Nitrogen 6 max & sabre lite boards have used 1.2V for VDDSOC_IN, VDDARM_IN and VDDARM23_IN of the iMX6Q processor. But it is 1.375V in Freescale SabreSD board. What should be the correct voltage for this ?
Can anyone tell me the recommended voltages for processor power blocks ?
Nitrogen6_max
Sabre SD
Regards,
Peter.
Hi Peter
for i.MX6Q it is defined in Table 6. Operating Ranges i.MX6DQ Datasheet
http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf
and sect.8.4.3 Clocks at boot time i.MX6DQ Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
For other i.MX processors - in their datasheets.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------