What's the relationship between "capture" camera driver and "subdev" camera driver in kernel 3.14?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's the relationship between "capture" camera driver and "subdev" camera driver in kernel 3.14?

2,448 Views
dehuanxin
Contributor III

I'm studying ov5640_mipi camera driver in 3.14 kernel and trying to add a driver for a custom MIPI-CSI camera.

I see ov5640_mipi has two drivers in linux-fslc/drivers/media/platform/mxc/capture at 3.14-1.0.x-mx6 · Freescale/linux-fslc · GitHub and also in linux-fslc/drivers/media/platform/mxc/subdev at 3.14-1.0.x-mx6 · Freescale/linux-fslc · GitHub  .

It seems to me that the subdev driver is newly added in 3.14 and does not exist in 3.10, but thethe two share the same kernel config macro.

Question: if I want to add driver to support a custom MIPI-CSI camera, which one shall I use as a template?

Labels (2)
3 Replies

1,519 Views
igorpadykov
NXP Employee
NXP Employee

also CSI2IPU (MIPI CSI to IPU Gasket) is present only

for parts with IPU, so seems "subdev" camera (used with parts

without ipu) is useless for MIPI camera.

Best regards

igor

0 Kudos
Reply

1,519 Views
dehuanxin
Contributor III

Any idea how long will the capture driver be supported?

Mainline kernel has dropped v4l2 internal API in 3.14.

BTW isn't it insane to decide use it in the first place?

0 Kudos
Reply

1,519 Views
gary_bisson
Senior Contributor III

Hi,

To put it in a simple way, the capture driver is meant for platforms having/using the IPU (i.MX6Q, i.MX6QP, i.MX6DL etc...). Whereas the subdev is targeting the other platforms (i.MX6SL, i.MX6SX, i.MX7 etc...).

So depending on the platform you use, you have to pick one or the other driver.

Hope this helps.

Regards,

Gary

0 Kudos
Reply