What's the relationship between "capture" camera driver and "subdev" camera driver in kernel 3.14?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the relationship between "capture" camera driver and "subdev" camera driver in kernel 3.14?

2,858件の閲覧回数
dehuanxin
Contributor III

I'm studying ov5640_mipi camera driver in 3.14 kernel and trying to add a driver for a custom MIPI-CSI camera.

I see ov5640_mipi has two drivers in linux-fslc/drivers/media/platform/mxc/capture at 3.14-1.0.x-mx6 · Freescale/linux-fslc · GitHub and also in linux-fslc/drivers/media/platform/mxc/subdev at 3.14-1.0.x-mx6 · Freescale/linux-fslc · GitHub  .

It seems to me that the subdev driver is newly added in 3.14 and does not exist in 3.10, but thethe two share the same kernel config macro.

Question: if I want to add driver to support a custom MIPI-CSI camera, which one shall I use as a template?

ラベル(2)
タグ(4)
3 返答(返信)

1,929件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

also CSI2IPU (MIPI CSI to IPU Gasket) is present only

for parts with IPU, so seems "subdev" camera (used with parts

without ipu) is useless for MIPI camera.

Best regards

igor

0 件の賞賛
返信

1,929件の閲覧回数
dehuanxin
Contributor III

Any idea how long will the capture driver be supported?

Mainline kernel has dropped v4l2 internal API in 3.14.

BTW isn't it insane to decide use it in the first place?

0 件の賞賛
返信

1,929件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

To put it in a simple way, the capture driver is meant for platforms having/using the IPU (i.MX6Q, i.MX6QP, i.MX6DL etc...). Whereas the subdev is targeting the other platforms (i.MX6SL, i.MX6SX, i.MX7 etc...).

So depending on the platform you use, you have to pick one or the other driver.

Hope this helps.

Regards,

Gary

0 件の賞賛
返信