What's the difference of UUU and fastboot for i.mx linux?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's the difference of UUU and fastboot for i.mx linux?

706 Views
cnspring2002
Contributor II

I can use uuu to flash i.mx linux bootloader/images, like next:

 

SDP: boot -f imx-boot-flash_evk

 

SDPV: delay 100

SDPV: write -f imx-boot-flash_evk -skipspl

SDPV: jump

 

FB: ucmd setenv fastboot_dev mmc

FB: ucmd setenv mmcdev ${emmc_dev}

FB: umcd mmc dev ${emmc_dev}

FB: flash -raw2sparse all imx-image.wic

FB: flash bootloader imx-boot-sd.bin-flash_evk

 

I want to know after device going to "FB" status, can I use fastboot to replace bold part? I mean what's the advantage to use "UUU" compared to use "fastboot tool" after board already in FB status? Thanks.

 

Tags (1)
0 Kudos
Reply
1 Reply

665 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

The advantage of the UUU is that it uses ROM api to download bootloader with USB, with the help of which subsequent download functions, such as the fastboot command can be implemented. If there is no bootloader available in the emmc/sd card on the board, then the boot will not be able to start, and the UUU can use the USB to realize the writing in the empty emmc/sd card state. If you have booted on the board and entered uboot cmd then you can use fastboot., but it is not as easy as a few lines of commands in a uuu script.



Best Regards,
Zhiming

0 Kudos
Reply