What's the default configuration of CP15:C11:C1:1, PLEPCR, in IMX6 BSP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the default configuration of CP15:C11:C1:1, PLEPCR, in IMX6 BSP?

ソリューションへジャンプ
1,326件の閲覧回数
dehuanxin
Contributor III

I found in <ARM Cortex A8 TRM (ARM DDI 0388F)>, section 4.3.30, <Preload Engine Parameters Control Register>, that "PLE wait states" (PLEPCR[7:0]) can be used to limit the usage of PLD instructions.

What's it's reset value or default value in IMX6 BSP? And where shall I place the code that changes it during boot process, in U-BOOT or kernel?

0 件の賞賛
返信
1 解決策
1,237件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dehuan

Cortex-A9 processor is delivered as synthesizable RTL, please look at part of i.MX6DQ RM

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,238件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dehuan

Cortex-A9 processor is delivered as synthesizable RTL, please look at part of i.MX6DQ RM

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信