What's the best way to lock the MAC address in the OCOTP on the iMX6dq?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's the best way to lock the MAC address in the OCOTP on the iMX6dq?

1,690 Views
rockykrcatovich
Contributor I

What's the best way to lock the MAC address in the OCOTP on the iMX6dq? 

Tags (2)
0 Kudos
Reply
5 Replies

1,272 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )

Thank you for using Freescale Community.

1,272 Views
rockykrcatovich
Contributor I

Hello D,

I moved my post to the i.MX Community, it was there from Tuesday through yesterday, but today it seems to have disappeared.

Do you know where it could have moved to, or how I can find it?

Thanks,

Rocky

0 Kudos
Reply

1,272 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Rocky,

I would recommend looking at the code for MAC address programming test included on the i.MX6SDK (link below).

https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&fr=gtl&Parent_nod...

Look at apps/obds/src/test/program_mac_address.c

This should serve as a reference for programming the MAC address.

0 Kudos
Reply

1,272 Views
Wlodek_D_
Senior Contributor II

Hi Rocky,

Your post is still in i.MX Community (see hyperlink What's the best way to lock the MAC address in the OCOTP on the iMX6dq? or  https://community.freescale.com/thread/324113  ).

Rgds,

W.

0 Kudos
Reply

1,272 Views
rockykrcatovich
Contributor I

Thanks for the tip.

0 Kudos
Reply