What pull PMIC_ON_REQ signal up when i.MX6 PMIC_ON_REQ is low?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What pull PMIC_ON_REQ signal up when i.MX6 PMIC_ON_REQ is low?

Jump to solution
1,990 Views
satoshishimoda
Senior Contributor I

Hi community,

I want to confirm about i.MX6 PMIC_STBY_REQ behavior.

Actually, PMIC_STBY_REQ of i.MX6D is tied to STANDBY pin of MMPF0100 on our custom board.

And PMIC_STBY_REQ line is changed to high level when i.MX6D is in low power mode and PMIC_ON_REQ (tied to PWRON pin of MMPF0100) is low.

Then, I want to know which chip (i.MX6D or MMPF0100) pulls PMIC_STBY_REQ line to high.

Could you let me know it?

(e.g. i.MX6D SNVS pulls the line to high, MMPF0100 internal pull-up resistor changes it high)

Best Regards,

Satoshi Shimoda

Labels (4)
0 Kudos
1 Solution
1,201 Views
Yuri
NXP Employee
NXP Employee

PMIC_STBY_REQ is i.MX6 (actively driven) output. No need for pull up resistor, as for open drain signals. 

View solution in original post

0 Kudos
5 Replies
1,202 Views
Yuri
NXP Employee
NXP Employee

PMIC_STBY_REQ is i.MX6 (actively driven) output. No need for pull up resistor, as for open drain signals. 

0 Kudos
1,201 Views
satoshishimoda
Senior Contributor I

According to your reply, PMIC_STBY_REQ signal is always controlled by i.MX6, also in this case.

Is this right?

Best Regards,

Satoshi Shimoda

0 Kudos
1,201 Views
Yuri
NXP Employee
NXP Employee

Yes, let me remind the PMIC_STBY_REQ belongs to VDD_SNVS_IN (always ON) power group.

1,201 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

OK, I understand.

Thank you for your cooperation!

Best Regards,

Satoshi Shimoda

0 Kudos
1,201 Views
satoshishimoda
Senior Contributor I

Can somebody reply me?

0 Kudos