What maximum operating range of USB1_VBUS is support by i.MX8M Mini?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What maximum operating range of USB1_VBUS is support by i.MX8M Mini?

跳至解决方案
1,244 次查看
m_c
Senior Contributor I

In the page 18 i.MX8M Mini data sheet <http://nxp.com/doc/imx8mmiec>, it shows min/typ/max operating range of USB1_VBUS are 0.80/1.40/3.60v. In USB standard, VBUS is 5v. So what maximum operating range of USB1_VBUS is support by i.MX8M Mini?

标签 (1)
0 项奖励
回复
1 解答
1,144 次查看
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

datasheet is correct, usb connections are described in sect.3.9.14.1 Pad/Package/Board connections:


The USBx_VBUS pin cannot directly connect to the 5 V VBUS voltage on the USB2.0 link.
Each USBx_VBUS pin must be isolated by an external 30 K 1% precision resistor.

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,145 次查看
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

datasheet is correct, usb connections are described in sect.3.9.14.1 Pad/Package/Board connections:


The USBx_VBUS pin cannot directly connect to the 5 V VBUS voltage on the USB2.0 link.
Each USBx_VBUS pin must be isolated by an external 30 K 1% precision resistor.

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复