What kinds of SPI-NOR flash i.mx6q support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What kinds of SPI-NOR flash i.mx6q support

1,076 Views
carmilili
Contributor III

Hello everybody,

     To my produce,I want it to boot Linux OS from SPI-NOR flash.But I don't know what kinds of SPI-NOR flash i.mx6q support.

     Does if support all kinds of SPI-NOR flash or someone?

Labels (2)
0 Kudos
Reply
1 Reply

792 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

The IMX6 SPI boot was verified with M25P32-VMW6TG.

iMX6 can support boot from 2 or 3 byte addressing SPI NOR.

When you used 4 bytes addressing SPI NOR, as I know, as default, they will also work in 3 bytes addressing mode, after booted, the driver will switch the SPI NOR to 4 bytes addressing mode, then one thing should be noted: when reboot the board, the SPI NOR should also be reset to default 3 bytes address mode, otherwize, reboot will fail.

0 Kudos
Reply