What is the well tested platform for lollipop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the well tested platform for lollipop

545 Views
mutyalaraoneela
Contributor III

Hi All,

I am going to start building the latest version on Android lollipuop v5.1.1, Could you please guide me what is the platform that I  can start building for?

that is IMX6Sololite/Sabrelite or any other board is preferred? OR what is the mostly preferred platform for building images?

Regards,

Mutyala rao.

0 Kudos
Reply
1 Reply

458 Views
Yuri
NXP Employee
NXP Employee

Hello,

L5.1.1_2.1.0-ga release supports the "following platforms:

• Freescale i.MX 6Quad, and i.MX 6DualLite SABRESD board and platform

• i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform

• i.MX 6SoloLite EVK platform

• i.MX 6SoloX SABRE-SD board and platforms

• i.MX 6SoloX SABRE-AI board and platforms

• i.MX 7Dual SABRE-SD board and platforms


This release includes all Freescale porting and enhancements

based on Android open source code"

https://www.nxp.com/webapp/Download?colCode=IMX6_L5.1_2.1.0_ANDROID-DOCS&location=null&fpsp=1&WT_TYP...

https://www.nxp.com/webapp/Download?colCode=IMX6_L5.1_2.1.0_AND_SOURCE_BSP&appType=license&location=...

Summary Page :

Android OS for i.MX Applications Processors|NXP


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply